earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Operator Display
Functionalities: Administration, User Management
Product version: 3.3, 2022, 2023, 2024, 7.0
7/22/2021

User Configuration Screen

Use the User Configuration screen to configure the setttings for all users on this Operator Display.

 
action_zoom_plus_stroke User Configuration screen
Figure: User Configuration screen

Table: User Configuration Screen

Component

Description

Inactivity timeout

Tap - or + to edit the number of minutes of the inactivity timeout.

Lock user after

Tap - or + to edit the number of failed login attempts before the user is locked.

Lock user for

Tap - or + to edit the number of minutes during which the user is locked.

Characters

Tap - or + to edit the minimum number of characters required in passwords.

Lowercase characters

Tap - or + to edit the minimum number of lowercase characters required in passwords.

Numeric characters

Tap - or + to edit the minimum number of numeric characters required in passwords.

Special characters

Tap - or + to edit the minimum number of special characters required in passwords.

  • User Account Administration