earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Pojęcie

Pojęcie


Produkty: Operator Display
Funkcje: Harmonogramy
Wersja produktu: 3.3, 2022, 2023, 2024, 7.0
2021-07-22

Schedule Events

arrow1_rotationWeekly Events arrow1_rotationException Events arrow1_rotationSchedule Event Colors

A schedule has two types of events: weekly events and exception events. Weekly events occur every week at specified times. Exception events occur when the schedule deviates from the weekly schedule, such as during holidays. Exception events override the weekly events when there is an overlap.

Each schedule has a default value. The default value goes into effect after the exception events and weekly events are complete or relinquish control. Więcej informacji zawiera Viewing a Schedule Default Value .

For example, the weekly event for a fan ends at 17:00. The fan ran at a value of 3 (high) throughout the event. There are no scheduled events after the weekly event. Because you have assigned 0 as the default value, the fan adjusts to the default value and turns to 0 (off). The value remains at 0 until the next scheduled event.

Events occur in the following order of precedence:

  • Exception events

  • Weekly events

  • Default value

For example, the weekly event for a fan is set to On from '08:00 - 20:00'. An exception event is set to Off from '17:00 - 20:00' for a specifc date. The exception event overrides the weekly event so that the fan only runs from 08:00 to 17:00 on the specified date.

Weekly Events

A weekly event occurs every week for an extended period of time. You can schedule more than one weekly event for each day of the week.

Więcej informacji zawiera Weekly Events .

Exception Events

An exception event occurs instead of the scheduled weekly events for a single date, date range, or calculated date.

Więcej informacji zawiera Exception Events .

Schedule Event Colors

A schedule has a color code so you can identify weekly events and exception events at a glance. This color code can assist you when you are modifying your schedule or trying to troubleshoot any problems.

Więcej informacji zawiera Schedule Colors .

  • Schedule Handling
  • Weekly Events
  • Exception Events
  • Schedule Colors
  • Viewing a Schedule Default Value