earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Operator Display
Functionalities: Schedules
Product version: 3.3, 2022, 2023, 2024, 7.0
7/22/2021

Schedule Detail Screen

Use the schedule detail screen to view the detailed properties of the schedule.

 
action_zoom_plus_stroke Schedule detail screen
Figure: Schedule detail screen

Table: Schedule Detail Screen

Component

Description

Name

Displays the name of the schedule.

Description

Displays the description of the schedule.

Present value

Displays the current schedule output value. For more information, see Schedule Events .

Default value

Displays the schedule default value. For more information, see Schedule Events .

Effective Period

Displays the range of time the schedule is in service. For more information, see Schedule Events .

Priority for writing

Displays the priority at which the referenced properties are commanded. For more information, see BACnet Command Priorities .

  • Schedule Handling
  • Exception Event Priorities
  • Schedule Events
  • BACnet Command Priorities
  • Schedules Screen