earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Användargränssnitt

Användargränssnitt


Produkter: Operator Display
Funktionaliteter: Tidsscheman
Produktversion: 3.3, 2022, 2023, 2024, 7.0
2021-07-22

Schedule Detail Screen

Use the schedule detail screen to view the detailed properties of the schedule.

 
action_zoom_plus_stroke Schedule detail screen
Figur: Schedule detail screen

Tabell: Schedule Detail Screen

Component

Description

Name

Displays the name of the schedule.

Description

Displays the description of the schedule.

Present value

Displays the current schedule output value. Mer information finns i Schedule Events .

Default value

Displays the schedule default value. Mer information finns i Schedule Events .

Effective Period

Displays the range of time the schedule is in service. Mer information finns i Schedule Events .

Priority for writing

Displays the priority at which the referenced properties are commanded. Mer information finns i BACnet Command Priorities .

  • Schedule Handling
  • Exception Event Priorities
  • Schedule Events
  • BACnet Command Priorities
  • Schedules Screen