earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Användargränssnitt

Användargränssnitt


Produkter: Operator Display
Funktionaliteter: Grundläggande funktionalitet
Produktversion: 3.3, 2022, 2023, 2024, 7.0
2021-07-22

Outputs/Binary Detail Screen

Use the Outputs/Binary detail screen to display and edit the seleted binary output.

Varning Varning

Unintended equipment operation

Do not force values without knowing the effect.

Failure to follow these instructions can result in death, serious injury, or equipment damage.

 
action_zoom_plus_stroke Outputs/Binary detail screen
Figur: Outputs/Binary detail screen

Tabell: Outputs/Binary Detail Screen

Component

Description

Value

Tap Value to enable this output.

Force

Tap Force to override the value received from the device. Mer information finns i Value Editing .

  • Value Editing