Produkty: Operator Display
Funkcje: Podstawowa funkcjonalność
Wersja produktu: 3.3, 2022, 2023, 2024, 7.0
2021-07-22

Outputs/Analog Detail Screen

Use the Outputs/Analog detail screen to display and edit the values available for the seleted analog output.

Ostrzeżenie Ostrzeżenie

Unintended equipment operation

Do not force values without knowing the effect.

Failure to follow these instructions can result in death, serious injury, or equipment damage.

 
action_zoom_plus_stroke Outputs/Analog detail screen
Rysunek: Outputs/Analog detail screen

Tabela: Outputs/Analog Detail Screen

Component

Description

Value

Tap - or + to edit the value of the analog output.

Force

Tap Force to override the value received from the device. Więcej informacji zawiera Value Editing .

  • Value Editing