earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Operator Display
Functionalities: Engineering, BACnet/IP devices
Product version: 3.3, 2022, 2023, 2024, 7.0
7/22/2021

Network Setup Screen

Use the Network Setup screen to configure the IP network communication.

 
action_zoom_plus_stroke Network Setup screen
Figure: Network Setup screen

Table: Network Setup Screen

Component

Description

Static IP

Tap to use static IP address.

This task requires administrator permissions.

DHCP

Tap to use a DHCP server.

This task requires administrator permissions.

Connection state

Indicates if the network is online of offline.

IP address

Type the IP address.

This task requires administrator permissions.

Subnet mask

Type the subnet mask.

This task requires administrator permissions.

Gateway

Type the gateway.

This task requires administrator permissions.

  • Configuration