Produkty: Operator Display
Funkcje: Inżynieria, Urządzenia SmartX IP Controller
Wersja produktu: 3.3, 2022, 2023, 2024, 7.0
2021-07-22

Network Setup Screen

Use the Network Setup screen to configure the IP network communication.

 
action_zoom_plus_stroke Network Setup screen
Rysunek: Network Setup screen

Tabela: Network Setup Screen

Component

Description

Static IP

Tap to use static IP address.

This task requires administrator permissions.

DHCP

Tap to use a DHCP server.

This task requires administrator permissions.

Connection state

Indicates if the network is online of offline.

IP address

Type the IP address.

This task requires administrator permissions.

Subnet mask

Type the subnet mask.

This task requires administrator permissions.

Gateway

Type the gateway.

This task requires administrator permissions.

  • Configuration