earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Operator Display
Functionalities: Basic Functionality
Product version: 3.3, 2022, 2023, 2024, 7.0
7/22/2021

Inputs/Analog Detail Screen

Use the Inputs/Analog detail screen to display and edit the seleted input.

Warning Warning

Unintended equipment operation

Do not force values without knowing the effect.

Failure to follow these instructions can result in death, serious injury, or equipment damage.

 
action_zoom_plus_stroke Inputs/Analog detail screen
Figure: Inputs/Analog detail screen

Table: Inputs/Analog Detail Screen

Component

Description

Value

Tap - or + to edit the value of the analog input.

Force

Tap Force to override the value received from the device. For more information, see Value Editing .

  • Value Editing