earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Användargränssnitt

Användargränssnitt


Produkter: Operator Display
Funktionaliteter: Grundläggande funktionalitet
Produktversion: 3.3, 2022, 2023, 2024, 7.0
2021-07-22

Inputs/Analog Detail Screen

Use the Inputs/Analog detail screen to display and edit the seleted input.

Varning Varning

Unintended equipment operation

Do not force values without knowing the effect.

Failure to follow these instructions can result in death, serious injury, or equipment damage.

 
action_zoom_plus_stroke Inputs/Analog detail screen
Figur: Inputs/Analog detail screen

Tabell: Inputs/Analog Detail Screen

Component

Description

Value

Tap - or + to edit the value of the analog input.

Force

Tap Force to override the value received from the device. Mer information finns i Value Editing .

  • Value Editing