earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Hur göra

Hur göra


Produkter: Operator Display
Funktionaliteter: Tidsscheman
Produktversion: 3.3, 2022, 2023, 2024, 7.0
2021-07-22

Editing an Event Priority

You edit an event priority to change the exception event to a higher or lower priority.

To edit an event priority
  1. In Operator Display, on the Device List screen, tap the arrow button

     
    action_zoom_plus_stroke
    to select the device with the with the schedule event priority you want to edit.

  2. On the Device screen, tap the Schedules arrow button

     
    action_zoom_plus_stroke
    .

  3. On the Schedules screen, tap the schedule type arrow button

     
    action_zoom_plus_stroke
    .

  4. On the schedule view screen, tap the event you want to edit.

  5. On the event screen, tap + or - to edit the priority of the event. 1 is the highest priority and 16 is the lowest.

  6. Tap OK .

  7. On the schedule view screen, tap Save .

  • Exception Event Priorities