Produkty: Operator Display
Funkcje: Harmonogramy
Wersja produktu: 3.3, 2022, 2023, 2024, 7.0
2021-07-22

Edit Weekly Event Screen

Use the Edit weekly event screen to delete or change the details of a weekly event.

 
action_zoom_plus_stroke Edit weekly event screen
Rysunek: Edit weekly event screen

Tabela: Edit Weekly Event Screen

Component

Description

Value type

Displays the schedule type the event is added to. Więcej informacji zawiera Schedule Types .

Value

Tap - or + to edit the schedule output value when this event is active. Więcej informacji zawiera Weekly Events .

Inactive/Active

Tap Inactive or Active (On or Off) to edit the schedule output value when this event is active. Więcej informacji zawiera Weekly Events .

All day

Tap All day to make the event span 24 hours instead of selecting specific hours using From and To .

From

Tap - or + to edit the starting time of the event.

To

Tap - or + to edit the ending time of the event.

Days of week

Tap to select the day(s) of the week this event is active.

  • Schedule Handling
  • Weekly Events
  • Exception Events
  • Schedules Screen