Use the Edit date range exception screen to add, edit or delete the time span and the value of a date range exception.
Component |
Description |
Priority |
Tap + or - to edit the priority of the event. 1 is the highest priority and 16 is the lowest. For more information, see Exception Event Priorities . |
Start date ![]() |
Tap to select a specific start date or Now to select the current date. |
End date ![]() |
Tap to select a specific end date or Never to indicate the exception does not have an end date. |
Start time |
Displays the starting time of the event. |
End time |
Displays the ending time of the event. |
Value |
Displays the selected value of the event. |
![]() |
Tap to open the Edit exception event screen, where you add a time span and a value. For more information, see Edit Exception Event Screen . |
![]() |
Tap to open the Edit exception event screen, where you edit the time span and the value. For more information, see Edit Exception Event Screen . |