earth_america
user_standard Zaloguj się
action_search_stroke
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interfejs użytkownika

Interfejs użytkownika


Produkty: Operator Display
Funkcje: Harmonogramy
Wersja produktu: 3.3, 2022, 2023, 2024, 7.0
2021-07-22

Edit Date Range Exception Screen

Use the Edit date range exception screen to add, edit or delete the time span and the value of a date range exception.

 
action_zoom_plus_stroke Edit date range exception screen
Rysunek: Edit date range exception screen

Tabela: Edit Date Range Exception Screen

Component

Description

Component

Description

Priority

Tap + or - to edit the priority of the event. 1 is the highest priority and 16 is the lowest. Więcej informacji zawiera Exception Event Priorities .

Start date

 
action_zoom_plus_stroke

Tap to select a specific start date or Now to select the current date.

End date

 
action_zoom_plus_stroke

Tap to select a specific end date or Never to indicate the exception does not have an end date.

Start time

Displays the starting time of the event.

End time

Displays the ending time of the event.

Value

Displays the selected value of the event.

 
action_zoom_plus_stroke

Tap to open the Edit exception event screen, where you add a time span and a value. Więcej informacji zawiera Edit Exception Event Screen .

 
action_zoom_plus_stroke

Tap to open the Edit exception event screen, where you edit the time span and the value. Więcej informacji zawiera Edit Exception Event Screen .

  • Schedule Handling
  • Schedules Screen
  • Add Schedule Event Screen
  • Edit Exception Event Screen
  • Exception Events