earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Hur göra

Hur göra


Produkter: Operator Display
Funktionaliteter: Maskinteknik, SmartX IP-kontrollenheter
Produktversion: 3.3, 2022, 2023, 2024, 7.0
2021-07-22

Configuring the IP Network Communication

You configure the IP network communication to establish the IP network communication between Operator Display and the devices.

To configure the IP network communication
  1. In Operator Display, tap the menu button

     
    action_zoom_plus_stroke
    .

  2. On the menu, tap Settings .

  3. On the Operator Display Settings screen, tap Network .

  4. On the Network Setup screen, tap Static IP to use a static IP address or DHCP to use a DHCP server.

    Obs!

    When you select to use a DHCP server, the rest of the fields are automatically completed by the DHCP server and not editable.

  5. In the IP address box, type the static IP address for this Operator Display.

  6. In the Subnet mask box, type the subnet mask for this Operator Display.

  7. In the Gateway box, type the IP address of the gateway for this Operator Display.

  8. Tap OK .

  • Configuration
  • Network Setup Screen