earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Poradnik

Poradnik


Produkty: Operator Display
Funkcje: Inżynieria, Urządzenia SmartX IP Controller
Wersja produktu: 3.3, 2022, 2023, 2024, 7.0
2021-07-22

Configuring the BACnet/IP Network Communication

You configure the BACnet/IP network communication to establish the BACnet/IP network communication between Operator Display and the devices.

To configure the BACnet/IP network communication
  1. In Operator Display, tap the menu button

     
    action_zoom_plus_stroke
    .

  2. On the menu, tap Settings .

  3. On the Operator Display Settings screen, tap BACnet .

  4. On the BACnet Setup screen, in the Instance number box, type the intance number for this Operator Display.

  5. In the Port box, type the communication port number for this Operator Display.

  6. Tap Time master to configure Operator Display to send date and time to its connected devices.

  7. Tap OK .

  • Configuration
  • BACnet Setup Screen