earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Operator Display
Functionalities: Basic Functionality
Product version: 3.3, 2022, 2023, 2024
7/22/2021

Changing Password

You change a password to update your access to Operator Display.

Show More
action_close

Operator Display authenticate users via user name and password.

The system administrator creates a user account with your needed permissions so you can access Operator Display and perform your assigned tasks. For more information, see Logging on to Operator Display .

Notice

POTENTIAL COMPROMISE OF SYSTEM AVAILABILITY, INTEGRITY, AND CONFIDENTIALITY

  • Wipe screen after use to avoid fingerprints from password entry remaining on the screen.

  • Do not share accounts between multiple users.

Failure to follow these instructions can result in loss of data or equipment damage.

There are three different types of users in Operator Display:

Administrator

A building manager who has complete access to the configuration of the Operator Display, including user administration.

Technician

A maintenance person or janitor who uses the Operator Display to interact with devices without being able to modify the configuration.

Viewer

A security guard who can view Operator Display features like alarms, but is not authorized to perform actions.

Passwords

The minimum number of characters and how many lowercase, numeric, and special characters that are required when you create a password depends on how the Operator Display user settings are configured.

When you change your password, the password requirements for the Operator Display are displayed on the Change password screen. For more information, see Changing Password .

The following special characters can be used:

!*#$%'()*+-/:;<=>?@[\]^_'{|}~

User Administration

As an administrator you add and delete user accounts, and configure user settings, such as password minimum requirements.

For more information, see User Account Administration .

To change a password
  1. In Operator Display, tap the menu button

     
    action_zoom_plus_stroke
    .

  2. On the menu, tap the user name.

  3. On the user profile screen, tap Change Password .

  4. On the Change password screen, in the Current password box, type your current password.

  5. In the New password box, type your new password.

    Note:

    The following special characters can be used:

    !*#$%'()*+-/:;<=>?@[\]^_'{|}~

  6. In the Confirm password box, type your new password a second time.

  7. Tap Save .

  • User Account Handling
  • User Profile Screen
  • Change Password Screen