earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Operator Display
Functionalities: Engineering, BACnet/IP devices
Product version: 3.3, 2022, 2023, 2024, 7.0
7/22/2021

BACnet Setup Screen

Use the BACnet Setup screen to configure the BACnet/IP network communication.

 
action_zoom_plus_stroke BACnet Setup screen
Figure: BACnet Setup screen

Table: BACnet Setup Screen

Component

Description

Instance number

Type the BACnet instance number.

This task requires administrator permissions.

Port

Type the communication port number.

This task requires administrator permissions.

APDU retries

Type the maximum number of times that an Application Protocol Data Unit shall be retransmitted

This task requires administrator permissions.

APDU timeout

Type the time in milliseconds that the driver will wait for a response from a device after sending a request.

This task requires administrator permissions.

APDU Segment timeout

Type the amount of time in milliseconds between the retransmission of an Application Protocol Data Unit segment

This task requires administrator permissions.

Force Priority Level

Tap + or - to configure the priority level at which the force actions will be applied. For more information, see Value Editing .

This task requires administrator permissions.

Time master

Tap to determine if Operator Display sets the time for all its connected devices.

This task requires administrator permissions.

Device name

Type a name unique to this device.

This task requires administrator permissions.

Device description

Type a description unique to this device.

This task requires administrator permissions.

  • Configuration
  • Value Editing