BACnet objects and devices have a variety of required and optional properties that are used for the purposes of identification, reliability indication, and configuration of the object or device, and for prioritization of write requests.
The supported BACnet objects in Operator Display are:
Analog Input Object Type
Analog Output Object Type
Analog Value Object Type
Binary Input Object Type
Binary Output Object Type
Binary Value Object Type
Device Object Type
Multi-State Input Object Type
Multi-State Output Object Type
Multi-State Value Object Type
Input |
Output |
Value |
Object_Identifier Object_Name Object_Type Present_Value Description Event_State Units Acked_Transitions Event_Time_Stamps Event_Message_Texts_Config |
Object_Identifier Object_Name Object_Type Present_Value Description Event_State Units Priority_Array Relinquish_Default Acked_Transitions Event_Time_Stamps Event_Message_Texts_Config |
Object_Identifier Object_Name Object_Type Present_Value Description Event_State Units Priority_Array Relinquish_Default Acked_Transitions Event_Time_Stamps Event_Message_Texts_Config |
Input |
Output |
Value |
Object_Identifier Object_Name Object_Type Present_Value Description Event_State Inactive_Text Active_Text Acked_Transitions Event_Time_Stamps Event_Message_Texts_Config |
Object_Identifier Object_Name Object_Type Present_Value Description Event_State Inactive_Text Active_Text Priority_Array Relinquish_Default Acked_Transitions Event_Time_Stamps Event_Message_Texts_Config |
Object_Identifier Object_Name Object_Type Present_Value Description Event_State Inactive_Text Active_Text Priority_Array Relinquish_Default Acked_Transitions Event_Time_Stamps Event_Message_Texts_Config |
Input |
Output |
Value |
Object_Identifier Object_Name Object_Type Present_Value Description Event_State Number_of_States State_Text Acked_Transitions Event_Time_Stamps Event_Message_Texts_Config |
Object_Identifier Object_Name Object_Type Present_Value Description Event_State Number_of_States State_Text Priority_Array Relinquish_Default Acked_Transitions Event_Time_Stamps Event_Message_Texts_Config |
Object_Identifier Object_Name Object_Type Present_Value Description Event_State Number_of_States State_Text Priority_Array Relinquish_Default Acked_Transitions Event_Time_Stamps Event_Message_Texts_Config |