earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Operator Display
Functionalities: Alarms
Product version: 3.3, 2022, 2023, 2024, 7.0
7/22/2021

Alarm Detail Screen

Use the alarm detail screen to display the alarm details and to acknowledge the alarm.

 
action_zoom_plus_stroke Alarm detail screen
Figure: Alarm detail screen

Table: Alarm Detail Screen

Component

Description

Device

Displays the name of the device.

Object name

Displays the name of the input, output or value that activated the alarm.

Object description

Displays the description of the input, output or value that activated the alarm.

Event state

Displays the event state of the current alarm state. For more information, see Alarm Handling .

Event state text

Displays the event state text corresponding to the alarm state. For more information, see Alarm Handling .

Transitions

Displays a table that lists all the alarm state changes that has occurred.

 
action_zoom_plus_stroke

Indicates an active alarm that is acknowledged. For more information, see Alarm Handling .

 
action_zoom_plus_stroke

Indicates an active alarm in the state Fault that is not acknowledged. For more information, see Alarm Handling .

 
action_zoom_plus_stroke

Indicates an active alarm in the state Alarm that is not acknowledged. For more information, see Alarm Handling .

 
action_zoom_plus_stroke

Indicates a reset alarm that is not acknowledged. For more information, see Alarm Handling .

Transition

Displays the transition type. For more information, see Alarm Handling .

Time

Displays the date and time of the most recent alarm state change.

Message

Displays the alarm message corresponding to the alarm state. For more information, see Alarm Handling .

Acknowledge

Tap to acknowledge the alarm. For more information, see Alarm Handling .

  • Alarm Handling