Use the Add weekly event screen to create a new weekly event for a selected analog, digital, multi-state or enumerated schedule.
Add weekly event screen
Component |
Description |
Value type |
Displays the schedule type the event is added to. For more information, see Schedule Types . |
Value |
Tap - or + to edit the schedule output value when this event is active. For more information, see Weekly Events . |
Inactive/Active |
Tap Inactive or Active (On or Off) to edit the schedule output value when this event is active. For more information, see Weekly Events . |
All day |
Tap All day to make the event span 24 hours instead of selecting specific hours using From and To . |
From |
Tap - or + to edit the starting time of the event. |
To |
Tap - or + to edit the ending time of the event. |
Days of week |
Tap to select the day(s) of the week this event is active. |