earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Operator Display
Functionalities: Schedules
Product version: 3.3, 2022, 2023, 2024, 7.0
7/22/2021

Add Calculated Date Exception Screen

Use the Add calculated date exception screen to create new calculated date exception events for the selected schedule of this device.

 
action_zoom_plus_stroke Add calculated date exception screen
Figure: Add calculated date exception screen

Table: Add Calculated Date Exception Screen

Component

Description

Priority

Tap + or - to edit the priority of the event. 1 is the highest priority and 16 is the lowest. For more information, see Exception Event Priorities .

Year

Tap - or + to select a specific year between 2020 and 2100 , or Any year .

Month

Tap - or + to select a specific month between January and December , Odd months , Even months , or Any month .

Week of month

Tap - or + to select a specific week between First and Fifth , Last , or Any .

Day of week

Tap - or + to select a specific day between Monday and Sunday , or Any day .

Start time

Displays the starting time of the event.

End time

Displays the ending time of the event.

Value

Displays the selected value of the event.

 
action_zoom_plus_stroke

Tap to open the Edit exception event screen, where you add a time span and a value. For more information, see Edit Exception Event Screen .

 
action_zoom_plus_stroke

Tap to open the Edit exception event screen, where you edit the time span and the value. For more information, see Edit Exception Event Screen .

  • Schedule Handling
  • Exception Events
  • Exception Event Priorities
  • Schedules Screen
  • Add Schedule Event Screen