earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Operator Display
Functionalities: Basic Functionality
Product version: 3.3, 2022, 2023, 2024, 7.0
7/22/2021

About Screen

Use the About screen to display more information on Operator Display.

 
action_zoom_plus_stroke About screen
Figure: About screen

Table: About Screen

Component

Description

Model

Displays the Operator Display part number.

Platform version

Displays current platform version number.

Application version

Displays the current firmware version number.

ETH1 MAC address

Displays the MAC address for the Ethernet interface.

BACnet Device Name

Displays the device name defined in the BACnet Setup screen. For more information, see Configuring the BACnet/IP Network Communication .

BACnet Device Description

Displays the device description defined in the BACnet Setup screen. For more information, see Configuring the BACnet/IP Network Communication .

Erase all data

Tap to erase the device list, logs, and users from the Operator Display. The only data remaining will be the firmware version and time setting.

This task requires administrator permissions.

  • Operator Display Overview
  • Hardening Specifics
  • Configuring the BACnet/IP Network Communication