earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Produits : AS-P-3, AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P
Fonctionnalités : Semantic
Version produit : 7.0
30/09/2025

Semantic Overview

arrow1_rotationSemantic Database arrow1_rotationOntologies arrow1_rotationSemantic Data and EWS arrow1_rotationLicensing arrow1_rotationSemantic Navigation arrow1_rotationConfigure EcoStruxure Building Automation System to use Semantic Tagging arrow1_rotationSemantic Engineering arrow1_rotationTenant Repository

The EcoStruxure Building Operation software supports a database solution for external storage of semantic information.

The semantic information is a contextual representation of a building that follows the Brick schema. It includes representation of building assets such as points, locations, and equipment.

The semantic information is configured in WorkStation, and the information is available in WorkStation and WebStation. The information is also available through EcoStruxure Web Services.

Semantic Database

EcoStruxure Building Operation uses a Sparql database, GraphDB from Ontotext, to handle semantic queries.

Pour plus d'informations, voir Semantic Database .

Ontologies

Semantic is based on ontologies.

Pour plus d'informations, voir Ontologies .

Semantic Data and EWS

The EWS metadata makes it possible to add semantic information to the EWS items, provided that the EBO object that is exposed by EWS is semantically described.

Semantic tagging is exposed using EWS.

Pour plus d'informations, voir Semantic Data and EWS .

Licensing

You can use a limited number of queries in the Graph database without a license. To be able to use the Graph database to its full extent a license is needed.

If you use an GraphDB on another location than the EBO default location, you have to aquire a license.

Semantic Navigation

You can navigate the semantic database using search and filter.

Pour plus d'informations, voir Semantic Navigation in WorkStation .

Pour plus d'informations, voir Semantic Navigation in WebStation .

Configure EcoStruxure Building Automation System to use Semantic Tagging

Use this workflow to configure EcoStruxure Building Automation system to use semantics.

Pour plus d'informations, voir Configure EcoStruxure Building Automation System to use Semantic Workflow .

Semantic Engineering

Semantic engineering is the process describing an EcoStruxure Building operation database using semantic s .

Pour plus d'informations, voir Semantic Engineering Overview .

Tenant Repository

You can create a semantic repository for each tenant. You do this in a system with multi tenants where you do not want the tenants to share their semantic information.

Pour plus d'informations, voir Tenant Repository .

  • Semantic Navigation in WorkStation
  • Semantic Navigation in WebStation
  • Semantic Database
  • Ontologies
  • Semantic Data and EWS
  • Configure EcoStruxure Building Automation System to use Semantic Workflow
  • Semantic Engineering Overview
  • Tenant Repository