earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-B, Edge Server, Device Administrator, AS-P
Functionalities: Security
Product version: 2024, 7.0
12/3/2024

CA Certificate Tab

Use the CA Certificate dialog box to manage CA certificates.

 
action_zoom_plus_stroke CA Certificate dialog box
Figure: CA Certificate dialog box

Table: CA Certificate dialog box

Component

Description

Issued To

Displays the name of the company or organization the CA certificate is issued to.

Issued By

Displays the name of the company or organization that has issued the CA certificate.

Expiration Date

Displays the date when the certificate expires.

Pre installed

Displays all pre installed certificates that are installed on the computer that runs Device Administrator. Pre installed certificates are indicated with a check mark.

Add

Click to add a new certificate.

Add root certificate

Click to browse to, and install, a root certificate.

Delete

Click to delete the selected certificate.

Show pre installed certificate

Select to display all pre installed certificates on the computer that runs Device Administrator.

Apply

Click to apply all changes done on the field server.

Discard

Click to discard all changes done on the field server.

  • CA Certificate Management