Produkty: AS-B, Enterprise Central, Enterprise Server, AS-P
Funkcje: Semantic
Wersja produktu: 2022
2022-03-23

Filtering on Located in Type Dialog Box

Use the Filtering on located in type dialog box to filter on the semantic item located in a type in the semantic model.

 
action_zoom_plus_stroke Filtering on located in type
Rysunek: Filtering on located in type

Tabela: Filtering on located in type

Component

Description

Type

Click to add a semantic items to filter on.

Self

Click to filter on this type of item with this label. No parents or children are displayed.

Located in

Click to filter on all semantic item that are located in the selected semantic item.

Contains

Click to filter on all semantic items that contains the selected semantic item.

Direct

Click Direct to filter on all immediate children in the semantic database.

All

Click All to filter on all children in the semantic database.

  • Semantic Navigation in WebStation
  • Semantic Navigator in WebStation
  • Semantic Filtering Item Menu
  • Filtering on Located in Item Dialog Box
  • Filtering on Item with Label Dialog Box
  • Filtering on Item with Reference Dialog Box