earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P
功能: Semantic
产品版本: 2023
2022/12/17

Adding a Semantic Item

You add a semantic item from the menu when you want a semantic item without any label or path.

显示更多
action_close

Semantic engineering is the process describing an EcoStruxure Building operation database using semantic s .

All engineering regarding semantics is done in WorkStation.

Semantic Engineering Workflow

Use this workflow to make a semantic description of your EcoStruxure Building Operation database.

有关更多信息,请参阅 Semantic Engineering Workflow .

To add a semantic item
  • In the Semantic engineering view, on the Semantic Engineering Menu , click the Add button.

The semantic item is created in the Semantic Engineering Table view.

  • Opening the Semantic Engineering View
  • Clearing the Semantic Editing Table View
  • Creating Semantic Objects using Drag and Drop
  • Adding a Semantic Point to the Semantic Model
  • Copying and Pasting a Semantic Item
  • Editing the Semantic Path
  • Changing the Class of a Semantic Item
  • Updating the Semantic Model