You can edit the semantic items in a number of ways.
Semantic labels are labels that helps to identify a semantic item. Semantic labels can be edited or removed. Semantic labels can also be replaced using Find and repalce.
For more information, see Adding or Editing a Label of a Semantic Item .
For more information, see Find and Replace Labels and Paths on Semantic Items .
Semantic relations are relations between semantic items.
For more information, see Removing a Relation Between Semantic Items .
The semantic path defines the relation between a semantic item and an EBO object. Semantic path can be changed or removed. Semantic paths can also be replaced using Find and repalce.
For more information, see Editing the Semantic Path .
For more information, see Find and Replace Labels and Paths on Semantic Items .
All semantic items are part of a class. You can change the class of a semantic item.
For more information, see Changing the Class of a Semantic Item .
Update the semantic model if you have added alarms or trend logs to an EBO object that already have a relation to a semantic item. When you update the semantic model the alarm and trend log is added to the semantic model.
For more information, see Updating the Semantic Model .