The MP-V provides the following combination of communication ports:
Two Ethernet ports
Two USB ports
One RS-485 port
The two Ethernet ports are labeled:
Ethernet 1
Ethernet 2
The two Ethernet ports are 10/100BASE-TX (RJ45) ports.
The Ethernet interface is IEEE 802.3 compliant.
When both Ethernet ports are enabled, they function as an onboard Ethernet switch. Disabling the second Ethernet port disables the switching function. The switching function enables flexible network topologies. 有关更多信息,请参阅 BACnet/IP Controller Network Topologies . The second port also provides a connection point for a laptop running the Commission mobile application.
有关更多信息,请参阅 Communication Port Wiring .
The two USB ports are of different types:
USB host port
USB device port
The USB host port is a USB 2.0 type-A port, which is rated 2.5 W. The USB host port is reserved for future use.
The USB device port is a USB 2.0 mini-B port. The USB device port is reserved for future use.
有关更多信息,请参阅 Communication Port Wiring .
The following description applies only for MP-V controllers with part numbers SXWMPV7AX10002 and SXWMPV9AX10002. 有关更多信息,请参阅 Differences Between MP-V Hardware Versions .
The RS-485 port is labeled:
RS-485 Com A
The RS-485 port is rated 2 W (24 VDC).
The RS-485 port is an RJ45 port. 有关更多信息,请参阅 RJ45 Pinout for the RS-485 Port of the MP-V Controller .
The RS-485 port can be configured to use one of the following two communication protocols for different types of networks:
Sensor bus
Modbus
The sensor bus is designed for communication with SpaceLogic Sensor devices. 有关更多信息,请参阅 MP-V Sensor Bus .
The Modbus (RTU) network can be used for communication with standard Modbus devices. 有关更多信息,请参阅 MP-V Modbus .
The RS-485 port can also be configured to support BACnet MS/TP network communication with the hosting server. 有关更多信息,请参阅 MP-V BACnet MS/TP Support .
有关更多信息,请参阅 Allocating Flexible Ports .
The RS-485 port is by default configured to use the following network communication protocol:
Sensor bus
有关更多信息,请参阅 Communication Port Wiring .