earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Basic Functionality
Product version: 2024, 7.0
12/3/2024

Backing up and Restoring using WebStation

You can backup and restore the server from WebStation.

Show More
action_close

A subset of backup and restore features are available in WebStation.

You can create backups of the server using WebStation. The backup can be downloaded and uploaded from the server.

Scheduled backup must be done using WorkStation.

For more information, see Backup .

To backup and restore
  1. Click WebStation, click Workspace menu .

  2. Click System .

  3. Click Backup and restore .

  4. In the Backup and restore dialog:

    • Click Backup to create a manually initiated backup.

    • Select a backup and click Restore to restore the server to the selected backup.

  • Backup and Restore Overview
  • Backup and Restore using WebStation
  • Uploading and Downloading a Backup using WebStation
  • Backup