Produits : AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Fonctionnalités : Fonctionnalité de base
Version produit : 2024, 7.0
03/12/2024

Backing up and Restoring using WebStation

You can backup and restore the server from WebStation.

Afficher plus
action_close

A subset of backup and restore features are available in WebStation.

You can create backups of the server using WebStation. The backup can be downloaded and uploaded from the server.

Scheduled backup must be done using WorkStation.

Pour plus d'informations, voir Backup .

To backup and restore
  1. Click WebStation, click Workspace menu .

  2. Click System .

  3. Click Backup and restore .

  4. In the Backup and restore dialog:

    • Click Backup to create a manually initiated backup.

    • Select a backup and click Restore to restore the server to the selected backup.

  • Backup and Restore Overview
  • Backup and Restore using WebStation
  • Uploading and Downloading a Backup using WebStation
  • Backup