This section provides the RJ45 pinout for the MP-V controller's RS-485 port.
The RS-485 port is labeled RS-485 Com A. For more information, see MP-V Communication Ports .
The labeling of the RS-485 port differs between different hardware versions of the MP-V controllers. For more information, see Differences Between MP-V Hardware Versions .
The wiring recommendations for the RS-485 port depend on the type of network the port is used for. For more information, see Communication Port Wiring .
RJ45 Pin |
Description |
1 |
Not connected |
2 |
TXEN |
3 |
RS485+ (A) |
4 |
+24 VDC |
5 |
Ground |
6 |
RS485– (B) |
7 |
+24 VDC |
8 |
Ground |