earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interfaz de usuario

Interfaz de usuario


Productos AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Funcionalidad básica, Seguridad
Versión del producto: 2024, 7.0
02/12/2024

General Tab

Use the General tab to rename the server, select the default logon domain, and to configure the password policy.

 
action_zoom_plus_stroke General tab
Figura: General tab

Tabla: General Tab

Component

Description

Server name

Click to rename the server.

Default log on domain

Select the default domain from the list.

Minimum number of hours between password changes

Enter the minimum number of hours required between password changes. To disable this feature, enter 0. In this case, users can change their passwords immediately.

Expiry

Select to limit the days a password is in effect. You then enter the number of days before compulsory password change. The value of 0 specifies that the password does not expire.

Password Reusage Count

Enter the number of passwords that have to be different before you can use the same password again. To disable this feature, enter 0.

Minimum Password Length

Enter the minimum number of characters allowed in a password. To disable this feature, enter 0.

Characters Difference

Enter the number of characters that must be different from the characters in the last password. To disable this feature, enter 0.

Repeating characters

Select true to allow repeating characters.

Minimum Lowercase Characters

Enter the minimum number of lowercase characters allowed in a password. To disable this feature, enter 0.

Minimum Uppercase Characters

Enter the minimum numbers of uppercase characters allowed in a password. To disable this feature, enter 0.

Minimum Numeric Characters

Enter the minimum of numeric characters allowed in a password. To disable this feature, enter 0.

Numeric In Word

Select to require that numeric characters cannot be the first or last character.

Minimum Special Characters

Enter the minimum number of special characters allowed in a password. To disable this feature, enter 0.

Special in Word

Select to require that special characters cannot be the first or last character.

  • Password Policy
  • Configuring the Password Policy
  • Configuring the Password Policy using WebStation