earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-B, Edge Server, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Alarms
Product version: 2024, 7.0
12/2/2024

User Actions Dialog Box

Use the User actions page to force a user to actions that are connected to the alarm.

 
action_zoom_plus_stroke User Actions dialog box
Figure: User Actions dialog box

Table: User Actions Dialog Box

Component

Description

Acknowledgement type

​Select the type of acknowledgement for the alarm.

For more information, see Acknowledgements .

Checklist

​Enter the checklist that belongs to the alarm.

For more information, see Checklists .

Cause note group

​Enter the cause note group that is used by the alarm.

For more information, see Cause Notes .

Action note group

​Enter the action note group that is used by the alarm.

For more information, see Action Notes .

Required user action

​Select what actions the user has to perform when any of the listed events occur.

  • Acknowledgements
  • Alarm Functions
  • Create Alarm Wizard – User Action Page
  • Comments
  • Cause Notes
  • Action Notes
  • Checklists
  • Hide and Disable
  • Alarm Assignments