earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-B, Edge Server, Enterprise Server, AS-P, Project Configuration Tool
功能: 警报
产品版本: 2024, 7.0
2024/12/3

Editing a Cause Note using WebStation

You edit an existing cause note to change the name or the descriptions, or add the cause note to another cause note group.

显示更多
action_close

A cause note specifies the problem that caused the alarm. Cause notes are grouped by category, with possible alarm causes listed in each group. When an alarm is triggered, you can easily report the causes that triggered the alarm by selecting the predefined choices.

 
action_zoom_plus_stroke Cause Notes dialog box
图: Cause Notes dialog box

Reporting the cause of the alarm is either voluntary or mandatory. You can configure the alarm so the user is required to report the causes when certain events occur, such as when an alarm is disabled.

​Cause notes can be of great use the next time the same alarm is triggered or when extracting alarm statistics.

To edit a cause note using WebStation
  1. In WebStation, select an alarm object.

  2. In the alarm dialog box, click User actions .

  3. In the Cause Notes properties, click the Edit button

     
    action_zoom_plus_stroke
    .

  4. Click the cause note group.

  5. Click the Edit button

     
    action_zoom_plus_stroke
    or type direct in the text field for the cause.

  6. Click Save .

  • Alarm Functions
  • Alarms Overview
  • User Actions
  • Cause Notes
  • Creating a Cause Note using WebStation
  • Adding a Cause Note to an Alarm in WebStation
  • Configuring Forced User Actions using WebStation