earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Hur göra

Hur göra


Produkter: AS-B, Edge Server, Enterprise Server, AS-P, Project Configuration Tool
Funktionaliteter: Larm
Produktversion: 2024, 7.0
2024-12-03

Creating an Action Note using WebStation

You create an action note to connect it to an alarm, and to simplify the reporting of actions taken when correcting the problem that triggered the alarm.

Visa mer
action_close

​Action notes are grouped by category, with possible actions that may correct the problem listed in each category. An action note specifies the actions that you used to correct the problem that caused the alarm.

 
action_zoom_plus_stroke Action Notes dialog box
Figur: Action Notes dialog box

Reporting the actions that were taken is either voluntary or mandatory. You can configure the alarm so the user is required to report the actions when certain events occur, such as when an alarm is disabled.

​Action notes can be of great use the next time the same alarm is triggered or when extracting alarm statistics.

To create an action note using WebStation
  1. In WebStation, select an alarm object.

  2. In the alarm dialog box, click User actions .

  3. In the Action notes properties, click the Edit button

     
    action_zoom_plus_stroke
    .

  4. Do one of the following:

    • Select the action note group where you want to create the action note and then click Add to add an action note.

    • Click the Add button

       
      action_zoom_plus_stroke
      to create a new action note group and then click Add to add an action note.

  5. Click Save .

  • Alarm Functions
  • Alarms Overview
  • User Actions
  • Editing an Action Note using WebStation
  • Adding an Action Note to an Alarm using WebStation
  • Configuring Forced User Actions using WebStation