earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Как

Как


Продукты: AS-B, Edge Server, Enterprise Server, AS-P, Project Configuration Tool
Функции: Сигналы тревоги
Версия продукта: 2024, 7.0
03.12.2024

Editing an Action Note using WebStation

You edit an existing action note to change the name or the descriptions, or to add the action note to another group.

Показать больше
action_close

​Action notes are grouped by category, with possible actions that may correct the problem listed in each category. An action note specifies the actions that you used to correct the problem that caused the alarm.

 
action_zoom_plus_stroke Action Notes dialog box
Рисунок: Action Notes dialog box

Reporting the actions that were taken is either voluntary or mandatory. You can configure the alarm so the user is required to report the actions when certain events occur, such as when an alarm is disabled.

​Action notes can be of great use the next time the same alarm is triggered or when extracting alarm statistics.

To edit an action note using WebStation
  1. In WebStation, select an alarm object.

  2. In the alarm dialog box, click User actions .

  3. In the Action Notes properties, click the Edit button

     
    action_zoom_plus_stroke
    .

  4. Click the action note group.

  5. Click the Edit button

     
    action_zoom_plus_stroke
    or type direct in the text field for the action note.

  6. Click Save .

  • Alarm Functions
  • Alarms Overview
  • User Actions
  • Creating an Action Note using WebStation
  • Adding an Action Note to an Alarm using WebStation
  • Configuring Forced User Actions using WebStation