earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-B, Edge Server, Enterprise Server, AS-P, Project Configuration Tool
功能: 警报
产品版本: 2024, 7.0
2024/12/3

Editing a Checklist using WebStation

You edit a checklist to change the description of a step, or to rearrange the step order.

显示更多
action_close

A checklist is a set of steps that guides the user to which action to take when an alarm is triggered. If an alarm goes to normal state, the corresponding checklist is also reset and each step has to be checked again.

Checklists can be voluntary or mandatory. You can force the user to check each step in the checklist before the alarm can be acknowledged.

To edit a checklist using WebStation
  1. In WebStation, select an alarm object.

  2. In the alarm dialog box, click User actions .

  3. In the Checklist properties, click the Edit button

     
    action_zoom_plus_stroke
    .

  4. Click the checklist.

  5. Click the Edit button

     
    action_zoom_plus_stroke
    or type direct in the text field for the checklist step.

  6. Click Save .

  • Alarm Functions
  • Alarms Overview
  • User Actions
  • Adding a Checklist to an Alarm using WebStation
  • Creating a Checklist using WebStation
  • Configuring Forced User Actions using WebStation