earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: Semantic
产品版本: 2024, 7.0
2024/12/3

Adding a Tenant Repository on the EcoStruxure Building Operation Server

You create a tenant repository to limit the semantic information to a specified group of users.

显示更多
action_close

You can create a semantic repository for each tenant. You do this in a system with multi tenants where you do not want the tenants to share their semantic information.

All semantic information is created in one main repository but the semantic data for each tenant is transferred to a specific tenant database. Using group permission, you can control the users that can access the information in the tenant database.

Each tenant repository contains a filter of the locations and equipment. The repository also contains user credentials for the database.

To Add a tenant repository on the EcoStruxure Building Operation server
  1. In WorkStation, in the System Tree pane, in the System folder, expand Semantics .

  2. Click Tenant repositories .

  3. Click the Add button

     
    action_zoom_plus_stroke
    .

  4. Enter a name for the tenant repository.

  5. Click Create .

  6. Click the Edit button

     
    action_zoom_plus_stroke
    .

  7. In the Locations field, select the semantic filter.

  8. In the Semantic DB user box, enter the name of the user in the Semantic database.

  9. Enter a password for the user.

  10. Confirm the password.

  11. Click OK .

  • Semantic Overview
  • Semantic Engineering Overview
  • Semantic Tenant Repository Workflow
  • Tenant Repository
  • Tenant Repositories Dialog Box
  • Tenant Repository Dialog Box
  • Populating a Tenant Repository
  • Connecting a User Group to the Tenant Repository