earth_america
user_standard 登录
action_search_stroke
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-B, Edge Server, Device Administrator, AS-P
功能: 许可证管理
产品版本: 2024
2024/12/2

Removing Demo Licenses File from Device Administrator

You return demo licenses after they have expired or when you commission a site.

Do not remove the demo licenses file from Device Administrator until all demo licenses are removed from your field servers.

显示更多
action_close

Use this workflow to return demo licenses from field servers.

Related information can be found in the sections after the flowchart.

 
action_zoom_plus_stroke Return demo licenses from field servers workflow
图: Return demo licenses from field servers workflow
Return demo licenses from field servers

Return the demo licenses from your automations servers using Device Administrator.

You must return all the demo licenses from the field servers before you remove the demo license from Device Administrator.

有关更多信息,请参阅 Removing Demo Licenses File from Device Administrator .

有关更多信息,请参阅 Returning All Demo Licenses from the Selected Field Servers .

Do not remove the demo licenses file from Device Administrator until all demo licenses are removed from your field servers.

Remove demo licenses file from Device Administrator

When you have returned all demo licenses from your field server you can remove the demo licenses file from Device Administrator if you are not going to use the demo license again.

有关更多信息,请参阅 Removing Demo Licenses File from Device Administrator .

To remove a demo license file from Device Administrator
  1. In Device Administrator, click Entitlements .

  2. In the Entitlements view, click Demo License .

  3. Click Delete .

  4. Click the Save current list button

     
    action_zoom_plus_stroke
    .

You must now purchase, assign, and activate licenses for the features you want to use.

有关更多信息,请参阅 Field Server Licensing on Field Servers Connected to Internet Workflow .

  • Demo Licensing Overview
  • Return Demo Licenses from Field Servers Workflow
  • Returning Demo Licenses from Field Servers
  • Returning All Demo Licenses from the Selected Field Servers
  • Licenses View
  • Unable to Activate or Return a EcoStruxure Building Operation Software License