Produits : WebStation
Fonctionnalités : Fonctionnalité de base
Version produit : 2024, 7.0
03/12/2024

Displaying a List of Forced Values in WebStation

You display a list of forced values so that you can unforce them or set a timeout on them. From the Forced value list, you can unforce or set a timeout on a forced value.

Afficher plus
action_close

Diagnostics in WebStation is a method of check the health of your system. Using Diagnostics you can also resolve several issues in the system, for example unconfigured trend log and forced values. You can check the following using diagnostics in WebStation:

  • Disabled alarms

  • Objects in the system that require change control

  • Offline or invalid devices

  • Objects that require uploading or downloading to be synchronized with the current configuration

  • Forced values

  • Communication issues between servers

  • Unconfigured and stopped trendlogs

  • Time and time zone settings

  • Logged in users

  • Zoning issues

To display a list of forced values in WebStation
  1. In WebStation, click the Workspace menu.

  2. Expand the server.

  3. Click System .

  4. In the List view, click Diagnostics .

  5. Click Forced values .

  • Forced Values
  • Forced Values List in WebStation
  • Forcing a Value
  • Releasing a Forced Value
  • Setting a Timeout on a Forced Value WebStation