Produits : AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P
Fonctionnalités : Alarmes
Version produit : 2024, 7.0
03/12/2024

Displaying a List of Disabled Alarms in WebStation

You display all disabled alarms so that you can identify the alarms that might be enabled. You can enable the alarm from the list.

Afficher plus
action_close

Diagnostics in WebStation is a method of check the health of your system. Using Diagnostics you can also resolve several issues in the system, for example unconfigured trend log and forced values. You can check the following using diagnostics in WebStation:

  • Disabled alarms

  • Objects in the system that require change control

  • Offline or invalid devices

  • Objects that require uploading or downloading to be synchronized with the current configuration

  • Forced values

  • Communication issues between servers

  • Unconfigured and stopped trendlogs

  • Time and time zone settings

  • Logged in users

  • Zoning issues

To display a list of disabled alarms in WebStation
  1. In WebStation, click the Workspace menu.

  2. Expand the server.

  3. Click System .

  4. In the List view, click Diagnostics .

  5. Click Devices .

  • Diagnostics in WebStation
  • Diagnostics Alarms List in WebStation
  • Disable and Enable Alarms