earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Comment faire pour

Comment faire pour


Produits : Edge Server, Enterprise Central, Enterprise Server, AS-P
Fonctionnalités : Gestion des utilisateurs
Version produit : 2024, 7.0
03/12/2024

Displaying a List of User Sessions in WebStation

You display a list of user sessions in WebStation so that you can identify the users that are logged on to the system. From the list you can end a user session.

Afficher plus
action_close

Diagnostics in WebStation is a method of check the health of your system. Using Diagnostics you can also resolve several issues in the system, for example unconfigured trend log and forced values. You can check the following using diagnostics in WebStation:

  • Disabled alarms

  • Objects in the system that require change control

  • Offline or invalid devices

  • Objects that require uploading or downloading to be synchronized with the current configuration

  • Forced values

  • Meter objects that requires attention

  • Communication issues between servers

  • Unconfigured and stopped trendlogs

  • Time and time zone settings

  • Logged in users

  • Zoning issues

To display a list of user sessions in WebStation
  1. In WebStation, click the Workspace menu.

  2. Expand the server.

  3. Click System .

  4. In the List view, click Diagnostics .

  5. Click User .

  6. Click End user session if you want to end a user session.

  • Diagnostics in WebStation
  • Users List in WebStation
  • User Accounts and User Account Groups