earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: Edge Server, Enterprise Central, Enterprise Server, AS-P
功能: 用户管理
产品版本: 2023
2022/12/17

Displaying a List of User Sessions in WebStation

You display a list of user sessions in WebStation so that you can identify the users that are logged on to the system. From the list you can end a user session.

显示更多
action_close

Diagnostics in WebStation is a method of check the health of your system. Using Diagnostics you can also resolve several issues in the system, for example unconfigured trend log and forced values. You can check the following using diagnostics in WebStation:

  • Disabled alarms

  • Offline or invalid devices

  • Objects that require uploading or downloading to be synchronized with the current configuration

  • Forced values

  • Communication issues between servers

  • Unconfigured and stopped trendlogs

  • Time and time zone settings

  • Logged in users

  • Zoning issues

To display a list of user sessions in WebStation
  1. In WebStation, click the Workspace menu.

  2. Expand the server.

  3. Click System .

  4. In the List view, click Diagnostics .

  5. Click User .

  6. Click End user session if you want to end a user session.

  • Diagnostics in WebStation
  • Users List in WebStation
  • User Accounts and User Account Groups