earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Как

Как


Продукты: AS-B, Edge Server, AS-P, Project Configuration Tool, RP-C
Функции: Разработка, Зонирование
Версия продукта: 2023, 2024, 7.0
17.12.2022

Displaying a List of Zoning Issues in WebStation

You display a list of zoning issues so that you can identify zoning areas that need attention.

Показать больше
action_close

Diagnostics in WebStation is a method of check the health of your system. Using Diagnostics you can also resolve several issues in the system, for example unconfigured trend log and forced values. You can check the following using diagnostics in WebStation:

  • Disabled alarms

  • Objects in the system that require change control

  • Offline or invalid devices

  • Objects that require uploading or downloading to be synchronized with the current configuration

  • Forced values

  • Meter objects that requires attention

  • Communication issues between servers

  • Unconfigured and stopped trendlogs

  • Time and time zone settings

  • Logged in users

  • Zoning issues

To display a list of zoning issues in WebStation
  1. In WebStation, click the Workspace menu.

  2. Expand the server.

  3. Click System .

  4. In the List view, click Diagnostics .

  5. Click Zoning .

  6. In the list, click Verify and repair references .

  • Diagnostics in WebStation
  • Verify and Repair Zoning References
  • Diagnostics Zoning List in WebStation
  • Zoning in WorkStation and WebStation