earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P
功能: 警报, Sustainability, 趋势, 用户管理, 分区
产品版本: 2024
2024/12/4

Opening Diagnostics in WebStation

You open diagnostics in WebStation to check the health of your system.

显示更多
action_close

Diagnostics in WebStation is a method of check the health of your system. Using Diagnostics you can also resolve several issues in the system, for example unconfigured trend log and forced values. You can check the following using diagnostics in WebStation:

  • Disabled alarms

  • Objects in the system that require change control

  • Offline or invalid devices

  • Objects that require uploading or downloading to be synchronized with the current configuration

  • Forced values

  • Communication issues between servers

  • Unconfigured and stopped trendlogs

  • Time and time zone settings

  • Logged in users

  • Zoning issues

To open diagnostics in WebStation
  1. In WebStation, click the Workspace menu.

  2. Expand the server.

  3. Click System .

  4. In the List view, click Diagnostics .

  • Diagnostics in WebStation
  • Diagnostics Alarms List in WebStation
  • Diagnostics Devices List in WebStation
  • Diagnostics Downloadable List in WebStation
  • Forced Values List in WebStation
  • Diagnostics Server Communication List in WebStation
  • Diagnostics Time Configuration List in WebStation
  • Diagnostics Trendlogs List in WebStation
  • Users List in WebStation
  • Diagnostics Zoning List in WebStation