earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P
功能: 本地化
产品版本: 2024, 7.0
2024/12/3

Displaying a list of Time Configurations

You display a list of time configuration to see if you must synchronize servers. The list displays all servers that are not synchronized. Log on to Workstation to synchronize servers.

显示更多
action_close

Diagnostics in WebStation is a method of check the health of your system. Using Diagnostics you can also resolve several issues in the system, for example unconfigured trend log and forced values. You can check the following using diagnostics in WebStation:

  • Disabled alarms

  • Objects in the system that require change control

  • Offline or invalid devices

  • Objects that require uploading or downloading to be synchronized with the current configuration

  • Forced values

  • Meter objects that requires attention

  • Communication issues between servers

  • Unconfigured and stopped trendlogs

  • Time and time zone settings

  • Logged in users

  • Zoning issues

To display a list of time configurations
  1. In WebStation, click the Workspace menu.

  2. Expand the server.

  3. Click System .

  4. In the List view, click Diagnostics .

  5. Click Time configuration .

  • Diagnostics in WebStation
  • Diagnostics Time Configuration List in WebStation
  • Time and Time Zone Overview