earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AS-B, Edge Server, Device Administrator, AS-P
Functionalities: License Management
Product version: 2024
10/30/2025

Return Demo Licenses from Field Servers Workflow

Use this workflow to return demo licenses from field servers.

Related information can be found in the sections after the flowchart.

 
action_zoom_plus_stroke Return demo licenses from field servers workflow
Figure: Return demo licenses from field servers workflow
Return demo licenses from field servers

Return the demo licenses from your automations servers using Device Administrator.

You must return all the demo licenses from the field servers before you remove the demo license from Device Administrator.

For more information, see Removing Demo Licenses File from Device Administrator .

For more information, see Returning All Demo Licenses from the Selected Field Servers .

Do not remove the demo licenses file from Device Administrator until all demo licenses are removed from your field servers.

Remove demo licenses file from Device Administrator

When you have returned all demo licenses from your field server you can remove the demo licenses file from Device Administrator if you are not going to use the demo license again.

For more information, see Removing Demo Licenses File from Device Administrator .

  • Demo Licensing Overview
  • Field Server Demo License Management
  • Removing Demo Licenses File from Device Administrator
  • Returning Demo Licenses from Field Servers
  • Returning All Demo Licenses from the Selected Field Servers