earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AS-B, Edge Server, AS-P, Virtual Project Servers, RP-C
Functionalities: Engineering, Zoning
Product version: 2023, 2024
12/17/2022

Verify and Repair Zoning References

You can repair incorrect references between grouped segments.

For example, if you change the segment-object property Exclude after you have grouped the segments, the references between the segment objects will be wrong, according to the Exclude setting. Repair inspects the groups and repair the references between the segments if needed.

Verifying and repairing zoning references can be done using both WorkStation and WebStation.

Verify and Repair Zoning References using WebStation

Use Diagnostics in WebStation to display a list of incorrect zoning references. From the list you can repair the incorrect references using the Repair button.

You can also find the Verify and repair zoning references button in the zoning tool in WebStation.

For more information, see Displaying a List of Zoning Issues in WebStation .

Verify and Repair Zoning References using WorkStation

Use the Zoning tool in WorkStation to verify and repair zoning reference.

For more information, see Verifying and Repairing Zoning References .

  • Opening the Zoning Tool in WorkStation 
  • Opening the Zoning Tool in WebStation
  • Zoning Tool in WorkStation
  • Zoning Tool in WebStation
  • Verifying and Repairing Zoning References
  • Diagnostics in WebStation
  • Displaying a List of Zoning Issues in WebStation