earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: AS-B, Edge Server, AS-P, Project Configuration Tool, RP-C
功能: 工程, 分区
产品版本: 2023, 2024, 7.0
2022/12/17

Verify and Repair Zoning References

You can repair incorrect references between grouped segments.

For example, if you change the segment-object property Exclude after you have grouped the segments, the references between the segment objects will be wrong, according to the Exclude setting. Repair inspects the groups and repair the references between the segments if needed.

Verifying and repairing zoning references can be done using both WorkStation and WebStation.

Verify and Repair Zoning References using WebStation

Use Diagnostics in WebStation to display a list of incorrect zoning references. From the list you can repair the incorrect references using the Repair button.

You can also find the Verify and repair zoning references button in the zoning tool in WebStation.

有关更多信息,请参阅 Displaying a List of Zoning Issues in WebStation .

Verify and Repair Zoning References using WorkStation

Use the Zoning tool in WorkStation to verify and repair zoning reference.

有关更多信息,请参阅 Verifying and Repairing Zoning References .

  • Opening the Zoning Tool in WorkStation 
  • Opening the Zoning Tool in WebStation
  • Zoning Tool in WorkStation
  • Zoning Tool in WebStation
  • Verifying and Repairing Zoning References
  • Diagnostics in WebStation
  • Displaying a List of Zoning Issues in WebStation